Upgrading Project TGML Graphics
To upgrade TGML graphics to include the latest changes made to the graphics components from previous versions, do the following:
- Open Power Operation Studio.
- Navigate to Projects > Migration Tool > Power Operation Migration Tool.
- In the Power Operation Migration Tool, select the project you want to upgrade, and select the Update Reference Component Definitions checkbox.
- Click Migrate.
- Open Graphics Editor.
- Navigate to the Connection Debugger and click Create Configuration File.
The OneLineConfiguration.json file is updated to include the Advanced One-Line logic needed to support the latest updates for standard components.
NOTE: This upgrade process supports the standard components shipped with Power Operation. To upgrade custom components, open each component, make the required changes, and then save. Upon saving, the Reference Definition Update tool is initialized and updates the changes made to the referenced components within the TGML files in the currently selected project.